Auto Onboarding Portal

Submit your design for external onboarding

Name of the person submitting this design.
Letters, numbers, spaces, _ and - only (max 100 characters). Used for the qcstudio application entry and qcs_device_hub folder/branch.
Application category (maps to Categories. in applications.ts).
Comma-separated free text. Up to 15 tags, each max 40 characters. Rendered as a tags array in applications.ts.
Select an MCU kit to load its peripheral interfaces.
0 / 5 new peripherals added
Accepted format: a single .zip file (max 50 MB) generated using e2studio